Factory Automation

Training Course

Mitsubishi Electric Industrial Automation Training Academy

Mitsubishi Electric Industrial Automation Training Academy provides an excellent operational capability upskilling to the trainees where they can learn the topic of interest according to their level and applications. The training courses are conducted in a conducive environment for the trainees to learn and hands on with our latest products training kits. They are specially tailored for professionals, corporate clients and individuals from colleges, ranging from beginner to advance level.

Our comprehensive training courses will equip the necessary skillset and knowhow for each participant to advance to next level.

Meet our dedicated and experienced team of trainers to further develop the skills and competencies that is required in this transformation journey.

Tailoring doesn’t stop here, we have more up our sleeves

Our team of experienced trainers can design courses that are unique to your organization needs. If you need assistance to identify training needs or for group booking, please feel free to contact our trainer team: FA_service@asia.meap.com or call us at (65) 6470 2476

Send an inquiry

MELSEC Controller

Basic: MELSEC iQ-R programming (GX Works3) course

This course introduce and explains the basic hardware structure of Mitsubishi PLC products. It introduces the first basic steps of PLC programming using the GX Works3 PLC programming software.

Basic: MELSEC Q programming (GX Works2) course

This course introduce and explains the basic hardware structure of Mitsubishi PLC products. It introduces the first basic steps of PLC programming using the GX Works2 PLC programming software.

Advanced: MELSEC iQ-R programming (GX Works3) course

This course will run through the advanced features Mitsubishi PLC products. Concentrating on the applied instruction set, use the mathematical functions, displaying results and interfacing with analogue units.

Advanced: MELSEC Q programming (GX Works2) course

This course will run through the advanced features Mitsubishi PLC products. Concentrating on the applied instruction set, use the mathematical functions, displaying results and interfacing with analogue units.

Industrial Network

CC-Link IE Control course (GX Works3)

This course introduce and demonstrate the CC-Link IE Control network and its configuration, execution and troubleshooting.

CC-Link IE Field course (GX Works3)

This course introduce and demonstrate the CC-Link IE Field network and its configuration, execution and troubleshooting.

CC-Link course (GX Works3)

This course introduce and demonstrate the CC-Link network and its configuration, execution and troubleshooting.

MELSECNET / H course (GX Works2)

This course introduce and demonstrate the MELSECNET/H network and its configuration, execution and troubleshooting.

CC-Link IE Control course (GX Works2)

This course introduce and demonstrate the CC-Link IE Control network and its configuration, execution and troubleshooting.

CC-Link course (GX Works2)

This course introduce and demonstrate the CC-Link network and its configuration, execution and troubleshooting.

Industrial Robot

Robot Basic Course (MELFA FR/F series)

This course introduce Mitsubishi Electric robot products and the software needed to configure, teach points, make changes, and maintain a robot system

Robot Maintenance Course (MELFA FR / F series)

This course explain the basic maintenance structure of Mitsubishi Electric robot through lecture and hands on practice

AC Drive

AC Servo Basic Course (MELSERVO-J4)

This course introduce the MR-J4 series of AC Servo. It give a thorough knowledge of the features, hardware and parameters.

AC Servo Maintenance Course (MELSERVO-J4)

This course explain the basic maintenance structure and troubleshooting guide.

Inverter Basic Course (FREQROL-A800)

This course introduce the 800 series VFD. It give a thorough knowledge of the hardware and parameters.

Inverter Maintenance Course (FREQROL-A800)

This course explain the basic maintenance structure and troubleshooting guide.

Positioning Motion

Q Simple Motion (Positioning) Course (MELSERVO-J4)

This course introduce the motion control modules and the software needed to configure, make changes and maintain a motion system. Positioning, parameters, homing, diagnostics and synchronous control functions.

iQ-R Simple Motion Course (MELSERVO-J4)

This course introduce the motion control modules and the software needed to configure, make changes and maintain a motion system. Positioning, parameters, homing, diagnostics and synchronous control functions.

Q Motion Controller Course (MELSERVO-J4)

This course introduce the motion controller and MT Works2 software. Positioning, parameters, homing, diagnostics, real/virtual modes and camming features.

iQ-R Motion Controller Course (MELSERVO-J4)

This course introduce the motion controller and MT Works2 software. Positioning, parameters, homing, diagnostics, real/virtual modes and camming features.

Human Machine Interface

Basic: GOT Course (GOT2000)

The course explain the set-up and basic graphic objects that the HMI uses in conjunction with PLC devices. Programming of the HMI using GT Designer software and follow examples using the main features of the HMI.

Advanced: GOT Course (GOT2000)

This course introduce the GOT2000 Family of operator interface products and the software needed to create, configure and modify screens which can be used with PLC systems.